Editing meta-information Permalink

  1. Click “Project  Project Information”.

    The “Project Information” dialog opens.

  2. Click the “Summary” tab.

  3. Specify your data in the input fields (example: ‎0.0.0.1‎ in the “Version” input field).

    CODESYS creates a property with a key for each given value and manages them on the “Properties” tab. For a library project, CODESYS still uses the properties and sorts later in the library repository.

    If you select the option for CODESYS to create a functions block for these properties, then you can access the properties programmatically.